News Releases

Mitsubishi Electric Receives Order for Taiwan's First STATCOM for Power StabilizationWill help to control and stabilize diversifying power grid and support adoption of renewable energy

FOR IMMEDIATE RELEASE No. 3603

Rendition of substation where Taiwan's first STATCOM will be installed


TOKYO, May 26, 2023 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its Taipei-based affiliate Shihlin Electric & Engineering Corporation has received an order from Taiwan Power Company for Taiwan's first* static synchronous compensator (STATCOM) for power grid stabilization. STATCOMs are devices that control and stabilize voltage in power systems by instantly providing reactive power.** The STATCOM from Mitsubishi Electric will be delivered to the Nanke Substation in Tainan and installed in a substation designed to blend in with its surrounding landscape and community.
With a rated capacity of ±200 megavolt-amperes (MVA), Mitsubishi Electric's system will contribute to the stable operation of the Tainan Science Park, where a number of factories produce semiconductors and display monitors. Delivery is scheduled for the first half of 2025 and the system is expected to begin operating in the first half of 2026.
Taiwan Power highly evaluated Mitsubishi Electric's extra-reliable, high-performance insulated-gate bipolar transistor (IGBT) integrated with the STATCOM, as well as Shihlin Electric's experience in delivering and constructing substations, which led the utility to place Taiwan's first order for a STATCOM.



  1. *As of May 26, 2023, according to Mitsubishi Electric's research
  2. **Power produced by the STATCOM that is used to stabilize voltage fluctuations, but is not actually consumed

Note

Note that the press releases are accurate at the time of publication but may be subject to change without notice.


Inquiry

Media contact

Customer Inquiries