News Releases
FOR IMMEDIATE RELEASE No. 3334
TOKYO, February 6, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that in collaboration with Japan's National Institute of Information and Communications Technology (NICT) it has developed technology for an extra-thin Ka-band (27 to 40 GHz) active electronically steered array antenna (AESA) featuring the world's thinnest* profile, less than three centimeters, to deliver high-speed inflight connectivity services via satellites at data rates beyond 100 Mbps. The company also announced that it has developed the antenna elements and, in collaboration with Tohoku University and Tohoku MicroTec Co., developed a radio-frequency integrated circuit (RF-IC) for an envisioned millimeter-wave V-band (40 to 75 GHz) AESA that will be capable of delivering inflight connectivity at even faster speeds.
Mitsubishi Electric's new Ka-band AESA is thin and small enough to be installed in any aircraft, regardless of its size, and it can operate even at high latitudes, which will allow passengers to enjoy on-demand streaming and other high-speed internet services on flights worldwide. Following further testing and demonstrations, the company plans to commercialize its Ka-band AESA after 2023 and a V-band AESA after 2027.
Rendition of Mitsubishi Electric's AESA
Structure of Mitsubishi Electric's millimeter-wave antenna
Mitsubishi Electric's three-dimensionally integrated millimeter-wave RF-IC
Note that the press releases are accurate at the time of publication but may be subject to change without notice.